Work voltage:26V
loudspeaker:20W 4Ω
volume:85%
The Loudspeaker stalled when playing some music.Like the 27.mp3.
The speaker stuck for 1 minute and 24 seconds of the music, then returned to normal after 400ms.
As can be seen from the current, there is no overpower.
I'll put the schematic down here.
Can you help me find the reason?
Best Wishs.