Part Number: PCM1690
Hi team,
Could you give us a spec for the DAC output impedance min/typical/max if available. It is needed to calculate calculate the gain.
Regards,
Hideki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM1690
Hi team,
Could you give us a spec for the DAC output impedance min/typical/max if available. It is needed to calculate calculate the gain.
Regards,
Hideki
Hi Hideki,
I do not have any data for the output impedance of the voltage output amplifier integrated in the PCM1690. I would estimate that the typical zo is about 10Ω.
While we do not specify Zo, we do specify the minimum load impedance, which is 5k-15kΩ depending if it is DC or AC coupled.
Thanks,
Paul
Hi Paul,
Do you means an effect of the output impedance can be ignored as the minimum load impedance is much higher than the output impedance?
Regards,
Hideki
Yes, the high output load requirements should minimize the impact of the output impedance.