This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6240-Q1: MICBIAS over current threshold

Part Number: PCM6240-Q1


Hi team,

MICBIAS over current threshold is specified as min 82mA at MICBIAS=9V.

Is this also applicable to MICBIAS =5V? 

I would like to know if MICBIAS over current at 5V is also protected up to 82mA.

regards,