Part Number: PCM1802
Hello,
Our customer is trying to replace A-company ADC with minimum modification of existing EE.
PCM1802 0dBFS input sensibility is 3.0Vpp at VCC=5V but previous ADC has 2.1Vpp.
On the specification input sensitivity is varied by VREF2 voltage, and on application circuit VCC pin connect to VREF2 pin.
Then VREF2 voltage range is limited 4.5V to 5.5V by VCC operating voltage.
Can we connect VREF2 pin to other voltage to adjust input sensitivity?
We know this configuration is not recommended on datasheet, it is own risk circuit design but PCM1802 first stage amplifier voltage gain can be simply function of VCC within absolute max spec?
Regards,
Mochizuki