This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am calibrating the tas2563 amp. but It is always getting failed.
Using the below command and attached the ftcfg file got from the TI.
factorytest -t 25 -c TUNINGMODE-TEST_TAS2563.ftcfg -v
and below is the result.
----------------------------------------------------------------------------------------------------------
android:/data # factorytest -t 25 -c TUNINGMODE-TEST_TAS2563.ftcfg -v
TI TAS2563 factory test calibration sequence V1.0
nArg = 1, argc = 6
Line = FTC_BYPASS=0
Line = TEST_DELTA_T=80
Line = CALIBRATION_TIME=2000
Line = VERIFICATION_TIME=4000
Line = CONFIGURATION=0
Line = CONFIGURATION_CALIBRATION=1
Line = DEV_ADDR=98
Line = RE_HI=7.975
Line = RE_LO=6.525
Line = F0_HI=924
Line = F0_LO=616
Line = Q_HI=1.704
Line = Q_LO=1.136
Line = T_HI=40
Line = T_LO=0
Line = SPK_T_MAX=100
Line = SPK_RE_TOL_PER=10
Line = PPC3_RE0=6.7
Line = PPC3_FWARP=891
Line = PPC3_BL=0.814
Line = PPC3_MMS=0.0667
Line = PPC3_RTV=63.4
Line = PPC3_RTM=566.7
Line = PPC3_RTVA=136
Line = PPC3_SYSGAIN=8.92
Line = PPC3_DEV_NONLIN_PER=1.5
Line = PPC3_DELTA_T_LIMIT=80
Line = PPC3_PIG=2
Line = PPC3_RE_ALPHA=0.0033
Line = FS_RATE=48000
Line = umg_SsmKEGCye=0x00,0x0d,0x3c,0x01
Line = iks_E0=0x00,0x0f,0x34,0x01
Line = yep_LsqM0=0x00,0x0f,0x40,0x01
Line = mcb_ZwiNgmaj=0x00,0x0f,0x44,0x01
Line = oyz_U0_ujx=0x00,0x0f,0x48,0x01
Line = kgd_OEldlc=0x00,0x10,0x14,0x01
ambient temperature = 25.0
factorytest configuration:
CALIBRATION_TIME = 2000
Speaker A characterization data:
SPKA SPK_T_MAX = 100.00
SPKA SPK_RE_TOL_PER = 10.00
SPKA SPK_RE_ALPHA = 0.0033
SPKA PPC3_RE0 = 6.70
SPKA PPC3_FWARP = 891.00
SPKA PPC3_BL = 0.814000
SPKA PPC3_MMS = 0.066700
SPKA PPC3_RTV = 63.40
SPKA PPC3_RTM = 566.70
SPKA PPC3_RTVA = 136.00
SPKA PPC3_SYSGAIN = 8.92
SPKA PPC3_DEV_NONLIN_PER = 1.50
SPKA PPC3_PIG = 2.000000
libVersion=0x10006
TAS2563 mixer command SEC_MI2S_RX Audio Mixer MultiMedia1 = 1.
factorytest: Can't find mixer. Please install tinymix.
TAS2563 mixer command TAS2563 IVSENSE ENABLE = 1.
factorytest: Can't find mixer. Please install tinymix.
factorytest: Can't play /data/vendor/pa_cal/silence.wav. Please install tinyplay.
factorytest: Started playback of /data/vendor/pa_cal/silence.wav
factorytest: /dev/tiload_node handle = 3
nbook=140, npage=45, nreg=124, pData[1]=0xb2, pData[2]=0xe7, pData[3]=0xed, pData[4]=0x0
nbook=140, npage=46, nreg=8, pData[1]=0x8f, pData[2]=0xdc, pData[3]=0x24, pData[4]=0x0
nbook=140, npage=47, nreg=108, pData[1]=0xf2, pData[2]=0x30, pData[3]=0xa1, pData[4]=0x0
nbook=140, npage=46, nreg=32, pData[1]=0xf2, pData[2]=0xb0, pData[3]=0x24, pData[4]=0x0
nbook=140, npage=46, nreg=40, pData[1]=0xae, pData[2]=0x8e, pData[3]=0x41, pData[4]=0x0
nbook=140, npage=48, nreg=24, pData[1]=0x99, pData[2]=0x1a, pData[3]=0xeb, pData[4]=0x0
nbook=140, npage=48, nreg=28, pData[1]=0x18, pData[2]=0xd, pData[3]=0x82, pData[4]=0x0
nbook=140, npage=47, nreg=112, pData[1]=0xd4, pData[2]=0x3, pData[3]=0x3a, pData[4]=0x0
nbook=140, npage=47, nreg=116, pData[1]=0x95, pData[2]=0x5d, pData[3]=0x90, pData[4]=0x0
nbook=140, npage=47, nreg=124, pData[1]=0xaf, pData[2]=0x90, pData[3]=0xbf, pData[4]=0x0
nbook=120, npage=12, nreg=40, pData[1]=0x0, pData[2]=0x0, pData[3]=0x0, pData[4]=0x0
factorytest: Stop playback.
TAS2563 calibration values:
DevA Re = 0.00 Ohm
DevA rms_pow = 0x00000000
DevA t_limit = 0x00000000
SPK A Calibration fail : Re is too low (limit: 6.53).
---------------------------------------------------------------------------------------------------------------------------------------
And i tried to access PPC3 tool but it is not showing any apps.
Please let us know what extra steps need to be followed for FTC.
Also referring the below docs
TAS2563 End System Integration Guide, and TAS2555, TAS2557, and TAS2559 Factory Test and Calibration Guide
Thanks.
Hi, Raghu,
Our team will take a look at this and will provide a response as soon as possible.
Best regards,
Luis Fernando Rodríguez S.
Hi Raghu,
I'll check about FTC results along with our driver support team.
Regarding PPC3, can you share the account you're using to log in? (you can send a private message with the address) I can check what are the apps you have been granted access.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Raghu,
You didn't had access to any of the software tools, I have granted you access to PurePath Console as well as TAS2563 app.
The FTC results show 0's for all values, it would seem like the device is not configured correctly. Have you tried to initialize the device using bin file? Is it working correctly?
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
PPC3 is Still not able to load the any apps.
what do you mean by "device is not configured correctly" ? we have used the .bin file shared by TI. and audio is working.
Thanks
Hi Raghu,
Are you using PPC3 within a corporate network? Can you confirm you're using w10 system? We've seen some cases were corporate firewalls are not letting PPC3 connect to the download servers. In that case is there a chance you can use a different network?
If audio is working OK, then perhaps the recording path is the one having problems during calibration. Can you share schematic and layout files if possible to discard any hardware issue?
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators