This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processors forum

Part Number: TMS320VC5502

Hello TI,

I am Tipu from NYBSYS Private Ltd ,  working with TMS320C5502 eZdsp  board and CCSv4 which comes with the CD. I download all the datasheet of TMS320VC5502 and study it. The dsp board and CCSv4 work with those source code comes with the CCSv4 example test like led, lcd-osd9616, enet, aic3204, enet, switch etc. All the exam works great with CCSv4 but this CCS version not compatibility with windows 10. Then I download the latest version of CCSv10 but there is not example code for TMS320VC5502 dsp board. So I try to run CCSv4 example code in CCSv10 but it's not work.

Our main focus is input audio in dsp board and process it with VOLIB and AEC-AER  and output the process data. But I can't input audio in dsp board because there are not enough source code for TMS320C5502, also facing some problem to work with VOLIB and AEC-AER C55x library. I need a guideline with some exam code for audio input and process with those library. I don't find enough document or support guideline from internet. 

Can you help me?

Regards

Tipu, Embedded Engineer

IoT Department

NYBSYS Private Ltd.