Part Number: DIX4192
Other Parts Discussed in Thread: SRC4392, SRC4382
Case No.: CS0423242
Short description: T.I.# DIX4192 interface to Audinate DANTE Brooklyn II cpu
Case details or comments:
I want to interface the T.I.# DIX4192 (Digital Audio Interface Receiver and Transmitter) to the Audinate DANTE Brooklyn II module (CPU). The Brooklyn II CPU will be the Master and the DIX4192 will be the Slave for both receive and transmit. Do I need an Asynchronous Sample Rate Converter to do this? And if so, could I use the T.I.# SRC4382 or the T.I.# SRC4392?
Also, is this part going to be around for awhile, or is it about to be placed on the "Not For New Designs" list?