Other Parts Discussed in Thread: PCM4104, , PCM3168A
Hello, friends!
Can I implement the reading of the ADC's TDM output using uart or SPI? I also need to use a DAC, in this case the PCM4104, so can I send the TDM messages using one of these interfaces?
One unrelated question: is there an ADC with similar features (SNR, number of bits, sampling speed) to the PCM1840, but with 6 or 8 channels?
Thanks!