This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3212EVM-U: TLV320AIC3212EVM-U

Part Number: TLV320AIC3212EVM-U


HI, When I connect the TLV320AIC3212EVM-U to a windows PC and start  CodecControl App I can play with the EVM using the example scripts. But when I connect the TLV320AIC3212EVM-U to an ubuntu PC, it gets detected as a sound card named "USB-miniEVM". So, when  I run the alsamixer command and select the soundcard to be USB-miniEVM instead of default sound card, I get the following error:-

Can you help me resolve it? Why can't I control the EVM parameters in ubuntu Linux ??