Other Parts Discussed in Thread: PCM4202, PCM4202EVM
Customer has complaints of the PCM4202 having large phase delays .
Setup:
1) Using PCM4202 eval board
2) Providing a quadrature signal Sin to L and cosine to R channel as Inputs
3) Fs = *KHz.
4) Sweeping frequency range 250Hz. to 2500Hz.
Issue:
1) See only 90 deg phase difference at 250 Hz. (due to quad signal inputs; thus, no phase delay between L and R)
2) See 180 deg phase difference at 2500 Hz. (seems to have an extra and unwanted 90 deg phase change)
Verified the following:
1) Input signal is not saturating ADC
2) Customer claims the source is NOT distorted (i.e., at 2500HZ no extra phase distortion other than the expected 90 deg)
Any ideas ?
-RON