Part Number: TAS5825M
Hello Experts,
Would you please review as attached?
https://tidrive.itg.ti.com/a/O_dm5Lf3ZvQp92b-/49772971-a9a5-4527-bd91-69bf8d422609?l
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS5825M
Hello Experts,
Would you please review as attached?
https://tidrive.itg.ti.com/a/O_dm5Lf3ZvQp92b-/49772971-a9a5-4527-bd91-69bf8d422609?l
Best Regards,
Fujiwara
Hi Yasushi Fujiwara,
May i know PVDD voltage for this application? Maximum output power and its load?
On my side, it is suggested to check:
1. PVDD decoupling cap, 4.7uF decoupling cap is not enough. Ti requests for 2*(22uF + 22uF +0.1uF) at least.
2. Voltage rating of PVDD decoupling cap: it is suggested to be larger than PVDD*1.35V
3. BST_A/B/C/D cap: it needs to be 0.47uF rather than 0.22uF. Please refer to the latest datasheet.
BR,
Alix
Hi Alix,
Thank you for feedback. Here is answer for your question.
- PVD=20V
- Po=2W@4ohm
I have question about boot-strap cap value. According to EVM, it is 0.22uF. But datasheet mentioned it is 0.47uF. Should customer refer to the datasheet?
Best Regards,
Fujiwara
Hi Yasushi Fujiwara,
Voltage rating for PVDD 20V is not enough, please follow the recommendation.
Understood your confuse but please use 0.47uF.
Please refer to the datasheet for the detailed explanation.
BR,
Alix Wan.