Part Number: PCM2900C
Hi team,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM2900C
Hi team,

Hi Ivy,
There are no separate drivers for Linux for this device but I believe the USB audio class is incorporated into the Linux OS so it should interface without needing any additional drivers. Our USB audio codecs are class type 1.
Best,
Zak
Hi Zak,
I'd like to check a question with you.
Can PCM2900C be recognized as working as an audio device as long as the UAC1.0-enabled driver is turned on the Linux system on the USB host side?
As I understand it, the Linux supports UAC1. Kernel Configuration UAC1 devices are supported by turning on "config_SND config_SND_USB_audio_".
Thank you!
Regards,
Ivy