We adopted the TAS 5760 amplifier for our AVAS product to generate the sound.
We met with 2 failure case /31 total which included the amplifier internal clock error be active for 3 hours and 15min.
After system ignition off-on, the issue can be recovered.
(It is happened on the field, not the development phase).
We manually inserted a temporary amplifier internal clock error, it pops up the error. after removing the injection error, the issue can be recovered.
The long duration of internal clock error is not expected from our design point of view since the error is non-latching error.
The issue was sporadic. It only happened once within 2 months.
We can’t reproduce with our HW units in our stock.
May we know if any suggestions / ideas / experiences from your side may be helpful for the issue correction?
If possible, a conference call with specific time slot for our explanation on the issue will be appreciated.
if so , kindly share your emails so that I will separately contact with you in private for meeting arrangement.
Thanks