Part Number: SRC4190-Q1
Hello, Team,
SRC4190-Q1 is capable of accepting TDM input with TDMI input while also inputting I2S via SDIN.
Based on this, our customer is thinking to use SRC4190-Q1 with a setting below:

If data is inputted to TDMI, would reference clock be BCKO?
Or, if it is set to slave mode, then reference clock will be generated from external CLK; therefore only inputting data is ok?
Thanks,
Masaru