Part Number: TAS2563
Hi tI team,
When I am debugging TAS2563, I cannot capture the step-back signal. How do I set it up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our team is looking into this and will have a response for you as soon as possible.
Best Regards,
Justin Beigel
Hi Justin,
Update ,I encountered the following problems when debugging TAS2563: 1. Mono mode, L channel input is normal, R signal has no sound. 2, SDOUT PIN has no data.
TAS2563-QFN32 Configuration.zip
Hi,
Default settings for input mixer is "Mono with time slot equal to I2C address offset", you can add this command to the script and you'll get mix of L and R:
w 98 08 7a
Regarding SDOUT, I was able to record from the EVM using your cfg. Where are you looking for SDOUT data? Have you tried recording from the EVM?
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators