Part Number: PCM2706C
Other Parts Discussed in Thread: PCM2704C
Hi
Just curious is HOST pin only for more internal LDO current provide to external ROM or some other function?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
HOST pin along with PSEL pin is dedicated to selecting the power source.This selection affects the configuration descriptor. While in bus-powered operation, the maximum power consumption from VBUS is determined by the HOST pin (pin21 for the PCM2704C/5C, pin 3 for thePCM2706C/7C). For self-powered operation, the HOST pin must be connected to VBUS of the USB bus with a pull-down resistor to detect attach and detach. (To avoid excessive, suspend current, the pull down should be a high-value resistor.) Table1 summarizes the power configuration select options

Regards,
AK