Hi team,
customer would like to know the range of Vuvp_ex of DRV632?
in the datasheet, only show the typical value, no minmum and maximum. can you help share these two value? thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our team is looking into this thread and will respond as soon as possible.
Best Regards,
Justin Beigel
Hi Betty,
There is no specification for max and min for UVP voltage. 1.25V is the value used for the formulas provided in the data sheet to set the external voltage divider, having a range of voltages instead of a typical value would make the configuration more complex.
There is no further data we can provide on this spec.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators