Part Number: LM4950
Other Parts Discussed in Thread: TS5A22364
Hi
When BYPASS is high, VOUT is only at 12V and there is no sound output.
When the BYPASS is shorted to GND, sound is output instead. Please help to confirm what is the problem?
When the Bypass pin is pulled low, there is sound output, but the sound is abnormal and noisy
- Pin 1:0.2V AC, 2V DC inputBypass pin
- Pin 2, 8:5.6V DC
- Pin 9:0V AC, 6V DC input