This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2X63EVM: How to Program the TAS2X63 EVM's XMOS Codec to Send I2S FSYNC Signal

Part Number: TAS2X63EVM

Hi Sirs,

We got a pulse signals of the FSYNC from the I2S output of the XMOS Codec on the TAS2X63 EVM. Would you pls advise how to program the XMOS Codec with PPC3 GUI to send 50% duty cycle of FSYNC following the I2S standard?

Wayne Chen
05/07/2021

  • Hi Wayne,

    Can you please reach out directly through email? The required tool is internal use only.

    Alternatively you could use external signals into the pin header.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators