Part Number: PCM1863
Hello,
In the data sheet I see no specification for the minimum Energysense threshold. However, the EVM only allows you to set it to -57dBFS. I want to set it to -72dBFS; however, I notice that i get constant interrupt triggers when i manually set the threshold to 0x00 0x08 0x3B. With some voltage divider changes I can make -60dBFS work in my design and I see proper signal detect functionality on the interrupt line.
Is there a reason that -57dBFS is the minimum available value for Energysense in the EVM? What is the minimum value that can be functionally used?
I am using a standard 24-bit signed level calculation, same as would be used for gain and it appears to match up with the tool generated values.
- Adam