This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3140: Function restrictions depending on the clock frequency

Guru 14810 points

Part Number: TLV320ADC3140

Hi,

I plan to use TLV320ADC3140 with Fs=8kHz, 3ch, 32bit.

Are there any functional restrictions such as some functions are not supported if the Fs is not high enough?

Thanks,

Koki