Other Parts Discussed in Thread: PCM2706C, PCM2706, PCM2704C, PCM2705C, PCM2705, PCM2704, TUSB2036
Hello,
I already read the PCM2707 (-C) datasheets, but the information given there is not fully clear.
1. Can I change the PCM2707 (2707C) IC S/PDIF output volume by setting the IC volume control HID commands thru its SPI bus?
The OS used – Win’ XP, iOS.
The iPhone, iPod can be used too.
iPhones work with the PCM270x chips:
https://hifiduino.wordpress.com/2013/06/15/apple-airport-express-usb-audio-output-mod/
Apple Airport Express USB Audio Output Mod
http://blog.jdslabs.com/?cat=57
2. What does mean the “Master volume control” mentioned in the
datasheet on the page 27? :
======================================
The built-in digital volume controller can be manipulated by an
audio-class-specific request from 0 to –64 dB in
steps of 1 dB. Changes are made by incrementing or decrementing one
step (that is, 1 dB) for every 1 / ƒS time
interval, until the volume level reaches the requested value. Each
channel can be set to a separate value. The
master volume control is not supported. A request to the master volume
is stalled and ignored. The built-in digital
mute controller can be manipulated by an audio-class-specific request.
A master mute control request is
acceptable. A mute control request to an individual channel is stalled
and ignored. The digital volume control
does not affect either the S/PDIF or I2S outputs (PCM2706C/7C only).
======================================
3. Again, what does mean ” The digital volume control does not
affect either the S/PDIF or I2S outputs (PCM2706C/7C only).”
So, the S/PDIF output volume by setting the PCM2707 volume control
commands thru its SPI bus will be operated in PCM2706/7 or not?
The "only" point is not clear here. "Only" yes, or only not?
Regards,
R. B.