Hello,
I am having an issue with the TPA3255. The amplifier does not output a signal. I implemented the PBTL configuration following the schematic given in the datasheet. My schematic looks like this:
Please note that there are two 100uF caps in series with AMP+ and AMP- drawn on the preamp page for DC decoupling. Double checked the schematic with the datasheet but can not see any mistake so far.
After setting RESET high, FAULT and CLIP_OTW are both going high, thus the device should enter normal operation mode. I supply a 1kHz sinus input signal but on amplifier output nothing happens. I can only see a saw tooth wave of a few mV. What could be wrong?
I can supply a screenshoot of the scope when I am back in my office.
Any help would be appreciated!
Greetings,
Raphael