Part Number: TPA3106D1
Hi:
I'm starting to design a guitar amplifier with TPA3106, and i have some questions about it.
First of all, what are the input signal levels that TPA3106 can work with... in the "Absolute max ratings" it says that INN and INP can be in the range of [-0.3V to VREG + 0.5V]. This means than i have to addapt my guitar signal with an input buffer to be as small as 0.3Vpp so it does not exceed the low limit?
Another question is about VREG... in TINA reference design, it si connected to a 4V source... but in datasheet i understood that the 4V were regultated by the TPA3106 itself... and in the EVM schemtatics it is directly AC coupled to ground... why then in TINA reference design there is a DC source there? In the simulation, if i remove that source from the reference design, the output wave is visibly afected by some noise and the output level decreses a lot:
However, in the EVM schematics the 4V source to VREG is missing.
What should i do?
Thanks in advance for the help!