This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When customer use PCM5242+TPA3251 device to devolpment audio amplifier, we find some problem:
1. when use below PFFB circuit , it can work well, but the R_Z ( R3.3ohm/1W) are burn up easily.
Another, when system shut dow, it exsit POP noise. pls. give some advise .
2. When use the PCM5242+TPA3251 and refer the new PFFB circuit as below , TPA3251 can't work, can you help to check ?
3. When TPA3251 set to BLT mode and for two channel woofer (4ohm), the PVDD is 32V. TPA3251 is easily to OCP . The ROC_ADJ set to 22Kohm. We can't find the reason.
Hi Justin
Thanks.
We have found the answer about question 2 and 3, but there is another question need to be solved.
When we use new PFFB circuit, the shutdown POP happened too. Can you give a way to solve it ?
Hi Justin
The input signal is as below ,pls. refer. When protection hanppen, the CLIP_OTW pin is also going high, but the FAULT pin going low, and TPA3251 shutdown one of the channel or two channel, it can't self clearing, It must be restarted.. Attachment is the SCH and the PCB LAYOUT, and a vedio include CLIP_OTW, FAULT pin waveform, would you pls. give some guidance to solve this problem ?
CH1. 2 DIFF INPUT
CH3 FAULT
CH2: CLIP_OTW
CH3: FAULT