This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HELLO:
SYSTEMS DESIGN FLOW:-
PCM2706C > PCM5102A > TPA6120A2
Kindly recommended wiring for the DAC PCM5102A to the HPA TPA6120A2. This is a split power supply \ 12V design.
Note the design works, however the auxiliary output is not balance.
The left speaker louder than the right speaker. Also on the headphone, right is weak!
Please provided recommended wiring for the DAC PCM5102A to the HPA TPA6120A2. Trying to get the optimal sound quality for these devices.
SCENARIOS:
1. DAC PCM5102A => HPA TPA6120A2 => Speaker
2. DAC PCM5102A => HPA TPA6120A2 => Headphones
Regards,
Neil Henry
IRAD LLC
Neil,
The schematic looks good. I think the current connection of xIN- is correct, although I'll double check.
However, you've mention that the right channel signal is weak even at the output of PCM5102A, have you verified that this device connections are OK? I can ask the responsible team of this device to take a look, if needed.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Ivan,
Thank you for the review.
I have double checked all the connection, however the same as before.
Kindly have the device team check-it-out, another set of eyes as you suggested!
Most appreciative!
Regards,
Neil Henry
IRAD