This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1865: Noise level in two series

Part Number: PCM1865

 Hi,

I have written an email directly to the support engineer, but my question hasn’t been answered yet.

I’m using PCM1865 in pdm mode to process data from digital microphone and send it to microprocessor ESP32. I use sample frequency 131kHz and PCM config as followed:

pcm_wirte_reg( PCM186X_REG_PAGE_SELECT, PCM186X_REG_RESET );           //Resetowanie PCM

 

pcm_wirte_reg( PCM186X_REG_PAGE_SELECT, 0x03 );                                   // select Page3

pcm_wirte_reg( PCM186X_REG_MIC_BIAS_CTRL, 0x00 );                           // 0x15

 

pcm_wirte_reg( PCM186X_REG_PAGE_SELECT, 0x00 );                                   // select Page0

pcm_wirte_reg( PCM186X_REG_PWDOWN_CONF, 0b01110001 );                       // 0x70 - standby

 

pcm_wirte_reg( PCM186X_REG_ADC1L_IN_SEL, 0b01000010 );                      // 0x06 - VIN1L2

pcm_wirte_reg( PCM186X_REG_ADC1R_IN_SEL, 0b01000010 );                      // 0x07 - VIN1R2

pcm_wirte_reg( PCM186X_REG_ADC2L_IN_SEL, 0b01000000 );                      // 0x08 - none

pcm_wirte_reg( PCM186X_REG_ADC2R_IN_SEL, 0b01000000 );                      // 0x09 - none

 

pcm_wirte_reg( PCM186X_REG_GPIO_1_0_FUNC, 0b00010001 );                     // 0x10 - GPIO0 and GPIO1 as DIGMIC_IN0 and DIGMIC_IN1

pcm_wirte_reg( PCM186X_REG_GPIO_3_2_FUNC, 0b00000001 );                     // 0x11 - GPIO2 as DIGMIC_CLK

pcm_wirte_reg( PCM186X_REG_GPIO_PULLDOWN, 0b00000000 );                     // 0x15

 

//pcm_wirte_reg( PCM186X_REG_DPGA_VAL_CH1_L, 0x00 );                        // 0x0F DPGA gain = 0dB (default)

//pcm_wirte_reg( PCM186X_REG_DPGA_VAL_CH1_R, 0x00 );                        // 0x16 DPGA gain = 0dB (default)

 

pcm_wirte_reg( PCM186X_REG_DPGA_CH_2_1_CTRL, 0xff );                   // 0x19 - DPGA manual config (set 0dB)

 

pcm_wirte_reg( PCM186X_REG_AUDIO_INTERFACE_FORMAT, 0b01000100 ); // 0x0B

pcm_wirte_reg( PCM186X_REG_TDM_OSEL, 0b00000000 );                          // 0x0C

pcm_wirte_reg( PCM186X_REG_TX_TDM_OFFSET, 0b00000001 );                     // 0x0D

pcm_wirte_reg( PCM186X_REG_RX_TDM_OFFSET, 0b00000001 );                     // 0x0E

 

pcm_wirte_reg( PCM186X_REG_DIN_RESAMP, 0b00000001 );                   // 0x1B

pcm_wirte_reg( PCM186X_REG_CLOCK_CONF, 0b00101110 );                   // 0x20

 

pcm_wirte_reg( PCM186X_REG_PLL_FRAC_JD_DIV_LSB, 0 );                   // 0x2C

pcm_wirte_reg( PCM186X_REG_PLL_FRAC_JD_DIV_MSB, 0 );                   // 0x2D

 

pcm_wirte_reg( PCM186X_REG_INT_CONF1, 0x00 );                               // 0x60

 

pcm_wirte_reg( PCM186X_REG_DSP_CTRL, 0b10011100 );                          // 0x71

 

pcm_wirte_reg( PCM186X_REG_DSP1_CLOCK_DIV,           0 );        // 0x21

pcm_wirte_reg( PCM186X_REG_DSP2_CLOCK_DIV,           0 );        // 0x22

pcm_wirte_reg( PCM186X_REG_ADC_CLOCK_DIV,            7 );        // 0x23

 

pcm_wirte_reg( PCM186X_REG_PLL_SCK_CLOCK_DIV, 1 );        // 0x25

pcm_wirte_reg( PCM186X_REG_MCLK_CLOCK_DIV,           3 );        // 0x26

pcm_wirte_reg( PCM186X_REG_MSCK_CLOCK_DIV,           63 );       // 0x27

 

pcm_wirte_reg( PCM186X_REG_PLL_P_DIV, 1 );                             // 0x29

pcm_wirte_reg( PCM186X_REG_PLL_R_DIV, 1 );                             // 0x2A

pcm_wirte_reg( PCM186X_REG_PLL_INT_JD_DIV, 8 );                        // 0x2B

 

pcm_wirte_reg( PCM186X_REG_PLL_CONF, 0b00000011 );                          // 0x28 - start PLL

vTaskDelay( 50 );

pcm_wirte_reg( PCM186X_REG_PWDOWN_CONF, 0b01110000 );                       // 0x70 – run

 

 

 

I have two types of PCM series 6ATG4 A93F and 48TG4 C240. The problem is that the noise level is dramatically higher in 48TG4 C240. I compare the noise with a plot in datasheet, which says that useful signal should be -120dB. I count and 6ATG4 A93F have about -140dB but 48TG4 C240 have -100dB which have significant impact on received data. I attach a time course and fft of these two types of PCM. These two elements were on the same PCB board and the same software configuration.

Best regards,

Konrad Koperek

  • Hi Konrad,

    Welcome to e2e. As you know, we have discussed this a bit via email and since the part is showing odd behavior, we will have to screen the part at our end in Quality lab to see if there was any defect w the part. I have requested the Field team to help expedite getting the return part to factory so that we can better answer the question.

    Since the config and the board is the same, we will have to suspect the part at the moment, knowing what we know. We will have the results published as soon as we can look at the defective part here.

    Thanks & Best regards,
    Ravi