Part Number: TPA3255
Other Parts Discussed in Thread: TPA3251,
Hi,
We are using the TPA3251 and TPA3255 in our commercial class D power amplifier product range.
Our design team place a strong emphasis on ensuring that our end users connected speakers are protected under all possible failures modes of the TPA chip.
We currently have a DC detection circuit that feeds into a protection relay that can remove the speaker from the circuit if a significant amount of DC is detected on the line.
We would like to consider removing the DC protection circuit and relay as it adds significant cost to our BOM.
On Page 19 of the TPA3255 datasheet it states the following:
"9.4.1.3 DC Speaker Protection
The output DC protection scheme protects a speaker from excess DC current in case one terminal of the
speaker is connected to the amplifier while the other is accidentally shorted to the chassis ground. Such a short
circuit results in a DC voltage of PVDD/2 across the speaker, which potentially can result in destructive current
levels. The output DC protection detects any unbalance of the output and input current of a BTL output, and in
the event of the unbalance exceeding a programmed threshold, the overload counter increments until its
maximum value and the affected output channel is shut down. DC Speaker Protection is disabled in SE mode
operation."
My questions are:
1) Is the above statement where a speaker wire touches the chassis the only mode of failure that is protects a speaker against DC?
2) Is there any protection against the high side and low side full bridge simultaneous failure (ie Drain Source Short) that would allow a large amount of DC to go to the speakers?
Or is this event so unlikely/impossible to occur that it’s not feasible to protect against?
Kind Regards,
Jesse