Other Parts Discussed in Thread: TAS5715, TAS5717, TAS5716, TAS5706B
I'm currently considering using the TAS5715 for a new design but I'm a bit confused as to what the data sheet states regarding line out.
It states
The TAS5715 provides headphone PWM out that can drive a headphone amplifier. This feature cannot be used
in lineout mode, because once the headphone is selected, the speaker is muted. See the headphone use model
diagrams on how to use the headphone feature and quite turn on and off.
It there a "lineout mode" register or is this saying it can not be used in a line out function like to a sub woofer output or line level where you would want the powered speakers to be playing at the same time as the line out
Also, I'm looking for an audio amp chip that uses I2S and can provide around 20watts per channel on 24V rail @8ohms(but can handle 4ohms) and provide a line/subwoofer output via PWM or analog. The TAS5715 looks to be a fit unless the pwm out only works when the speakers are muted. Any suggested amp chips would be greatly appreciated.
Thanks