Hi There,
We are planning to use PCM1860 ADC with electret condensor microphone (WM-64C) with sensitivity of -45dB for our application.
So microphone will generate output voltages in the range of around 5.6mV. But in the PCM1860 chip, it is specified that 2.1Vrms is full scale input voltage for single ended input.
my questions are
1) whether this 2.1Vrms is the ADC input voltage range (after PGA in the chip) or it is the maximum input that i can give at the input pins VINR/VINL
2) Since PCM1860 operates at single power supply of 3.3V, how we can give 2.1Vrms (around 5.6Vpp) to the chip?
3) Can i give microphone input in the range of millivolt directly to the ADC or do i need to add external preamplifier before giving to ADC pin VINL/R? or can i use internal PGA to convert this millivolt range to 2.1Vrms? if so then this 2.1Vrms should be the input of ADC block in the chip.
Please share your comments to proceed further with this chip selection.
Thanks & Regards,
Murugan