Part Number: TLV320AIC3268
Hi Ti,
We want to convert two I2S stereo(audio source is HDMI audio) audios and one line in stereo source to a single I2S TDM with multi-channel(3 stereo pairs: line in, hdmi in 1, hdmi in 2).
Please help check AIC3268 configurations. Block diagram as below:
All I2S interface are configured to 4-wire(BCLK,WCLK,DIN,DOUT)
According to AIC3268 datasheet. Using the offset programmability and the DOUT line 3-state feature.
I2S1 DOUT(from line(ADC convert)), I2S2 DOUT(from hdmi 1), I2S3 DOUT(from hdmi 2) all connect with Host CPU I2S DIN pin.
Additionally, I2S stereo input to AIC3268 as below:
Expected I2S TDM output from AIC3268 to host CPU as below:
Is it possible for AIC3268?
Thanks a lot.
BR,
Steven