This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LME49724: using dc servo to remove offset voltage on the outputs

Part Number: LME49724


See attached schematic of LME49724, with dc servo circuit to null dc offset voltage on the outputs.

The input to the LME49724 is the summation of two signals.

Note: I realize that I should add another 0.1uF cap across R55 (so it is the same as R54).

- Is this the correct way to implement a dc servo with the LME49724?  

- Is there a better choice of part to use for the dc servo than the LT1097S8?

Thank you