Part Number: TSW14J56EVM
Other Parts Discussed in Thread: ADC12J4000
Hello,
I am using the TSW14j56EVM along with the ADC12j4000 EVM to capture RF pulses. I have a trigger that sends a 1.8V signal to the data capture EVM at the same exact time as the RF pulses, but the first pulse seems to be entirely missed no matter what pulse width I use. I've used 1us up to 10us with the same result. You can see from the HSDC snapshot below that the first pulse is barely showing, but as I increase the pulse width past 1us that first pulse completely disappears and the second pulse moves even close to time 0. I tried to illustrate this with the second diagram. The first is a representation of the HSDC pro capture. The second is what I expected to see, which was more of the first pulse, but instead I see the third part of the diagram which is that the first pulse is still completely missing and the second pulse has shifted to the left in time.
Could you clarify if the external trigger works off a rising or falling edge? If it is the rising edge, would there be so much delay between receiving the signal and reading the data that you would miss a 10us or longer pulse? I've verified the trigger and RF signals through an oscilloscope and they're rising edge is within nanoseconds of each other.