Good morning,
I am currently an undergraduate student at the Democritus University of Thrace in Greece performing my dissertation thesis in the field of biomedicine. For this purpose, my colleagues and I, would like to develop a system of wearable sensors that will enable the continuous monitoring of vital biomedical parameters such as the body temperature, the blood pressure, the saturation of oxygen in blood, the hearth rhythm, as well as the electrocardiogram.
Based on past projects, I have in my disposal the products, but I do not know for sure if this is the appropriate for the conduction of the system as described above. To a greater level of detail, I have already the following products:
- ADS1293EVM
- TIVATM C SERIES TM4C123G LaunchPad Evaluation Kit EK-TM4C123GXL
- LMT70EVM (Temperature Sensor)
I will supply ADS1299, which is suitable as the AFE for the EEG and ECG applications. After searching I have found the electrodes that I will need for the ECG measurements, so I would like you to help me regarding the electrodes for the EEG measurements, which one do you suggest ??