This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: Assembly Stack-Up/Material Properties

Part Number: ADC12DJ5200RF


Need to model thermo-mechanical effects of this device in a custom circuit board packaging application.  Can you please provide the necessary material properties (young's modulus, CTE, thermal conductivity) for the elements within this part, including any materials bonding the elements together? 

Datasheet side profile shows part constructed from 3 primary elements: (1) lower laminate, (2) die, and (3) lid/cover.  Assuming there is some type of material bonding (1) to (3).

If specific properties/stack-up cannot be shared, effective material properties and description of their use can be substituted.

Thanks