Part Number: USB2ANY
如何才能保证DAC80508EVM和USB2ANY之间 进行正确的SPI通讯呢?
硬件电路已经连接好,如下图1所示。但DAC80508EVM GUI显示连接未成功,我猜想是与USB2ANY之间通讯没有正常进行。我要怎么设置USB 软件界面正确配置呢?如图2、3是需要配置的界面以及DAC读写时序图。



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Wang Yue,
I am going to forward your inquiry to DAC supporting team. They can help you better than our team.
Here is user's inquiry - translated
How to ensure correct SPI communication between DAC80508EVM and USB2ANY?
The hardware circuit has been connected, as shown in Figure 1 below. But the DAC80508EVM GUI shows that the connection is unsuccessful. I guess the communication with USB2ANY is not working correctly. How do I set the USB software interface to configure correctly? Figures 2 and 3 are the interfaces that need to be configured and the DAC read and write timing diagrams.
I am new to DAC and SPI communication, I hope to get help from your company, I would be very grateful.
Best,
Raymond
Hi Yue,
The USB2ANY does work with Windows 10, 64-bit. Let's close this thread and focus on your other thread:
Thanks,
Paul