Other Parts Discussed in Thread: AMC3306M25
Dear TI Team
The customer wants to use the AMC3306EVM to check the behavior when the HLDO_OUT pin is overloaded.
Checking the data sheet, it is stated that it can handle loads up to IH = 1mA as shown in the table below.
I want you to answer the following questions.
1. 1. The data sheet of AMC3306M25 (installed in AMC3306EVM) states that the external load should not be connected as shown below.
Does this mean that a load of 1mA or more should not be connected?
2. Will it be damaged when a load of 1mA or more is applied?
(The rated current of the HLDO_OUT pin was not specified)
Best Regards,
Y.Ottey