Hi,
There is a C driver available for this part?
Thanks,
Andrei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
There is only a header file available for this device which can be downloaded at the Product folder of the device under Design Development section.
Regards
Cynthia
Hi Cynthia,
I'm aware of that header; it is helpful, but It would be nice to publish the driver (which I assume was developed in some form to characterize the part) for such ADCt with unique features as the RMS and ZCD block inside.
Thanks,
Andrei
Andrei,
The only available files are found in the product folder.
The EVM GUI support exporting register address and content based on the current user configuration.
Regards
Cynthia