Other Parts Discussed in Thread: ADS1230, DAC1220, ADS1232, PCM1754
Hi,
Here is my setup: Load Cell Signal that spans -36mV to 36mV -> ADS1230 20 bit -> Microprocessor -> Send serial data that contains the digital code from ADS1230 over a wireless module -> AIR -> wireless module receiving serial digital code data -> microprocessor -> DAC1220 20 bit -> Original load cell signal
Here are my questions:
1) According to the spec sheet of ADS1230, I should be ok with a 20 bit AtoD like ADS1230 right?
2) ADS1230 have a gain of 64 or 128 PGA. Since the input voltage is amplified by this multiplier, the DAC1220 on the receiving end will receive this amplified signal. So how do I reconstruct the original signal without the 64 or 128x gain? Please advise.
3) I believe the gain from the ADS1230 will introduce an error since there will be rounding to the nearest digit after the 64x or 128x multiplication. Am I correct? Also, I should be getting another rounding error when I try to divide the DAC1220 output signal back down by 64x or 128x to get back my original load cell mV signal. Am I getting this wrong? Or the error will be small enough that it's negligible? How do I calculate this error?
Please let me know if I miss anything major.
I would appreciate it if anyone can respond to this.
Paul