Hi,
I have a custom PCB with an AMC7834 and a MSP430 microcontroller, which works fine for RF MMIC biasing in the lab. It is powered using a LDO from a +12V supply.
This PCB however was recently integrated in an instrument, and is behaving very oddly in this specific situation. It appears that the AMC7834 is suddenly resetting after several minutes of operation without (known) external cause for reset. the MSP430 is monitoring the general status, clamp, and alarm registers as well as the power state register. It only happens in the instrument, the same configuration of a lab power supply is working fine.
Without raising any alarm, it goes into low power mode, powers down PA_ON and engages the clamps. The sleep pins are disabled, reset driven high by the MSP430 (in addition to a 10k pullup). Monitoring of the 5V rail and input rail does not show any obvious dips, and should be picked up by the AMC monitoring as well.
It appears to be some kind of EMI issue, unless there's something I missed?
Is there any other way that would lead to a reset of the AMC?
Cheers,
Kai