Other Parts Discussed in Thread: ADS1100
Hello,
I am developping an application with a presure sensor and would like to use ADS1100 as A2D convertor. On the same I2C bus I have an EEPROM which work fine.
With the ads I had trouble :
- during initialisation (send the configuration byte), I see nothing wrong (ADS send the ACK as expected)
- config is as follow :
- PGA0 = 0 and PGA1 = 0 : gain = 1
- DR0 = 1 and DR1 = 1 : 8 samples per second
- SC = 1 : continuous mode
- other = 0
- when I start a read operation, ADS send the ACK and then the 3 bytes.
But all bytes equal 0xFF, even the config one.
Analog input is 4.1 V (Vin- = 0 V, Vin+ = 4.1 V).
That very disapointing and I am unable to see what is wrong. Any idea would help !
Thanks you
Jean-Marie