Part Number: DAC8574
The task is to generate output voltages between -2.048 and +2.048 V with a DAC8574. For this purpose the DAC is operated with +/- 2.5 V.
The I2C signals have a swing of 5 V referred to -2.5 V. The signal transmission with I2C works in principle, but the output voltages are shifted
by about 0.45V (2.5 - 2.048 = 0.452 ?). According to the data sheet, IOVDD only is responsible for the level of the digital inputs.
IOVDD is currently at +2.5 V (IOVDD connected to VDD), which should not have any influence on the analog outputs. Is this circuit wrong?
If IOVDD has an influence on the output voltage, must IOVDD be stabilized?