Hello,
I considering analog output circuit board that uses DAC8760.
I would like to know which of the following conditions is the thermal resistance value of junction to ambient in section 7.4 of the DAC8760 data sheet.
Condition 1: The condition that the thermal pad on the bottom of the package is connected to the copper plane of the board.
Condition 2: The condition that the thermal pad on the bottom of the package is not connected to the copper plane of the board.
If it is a characteristic of junction to ambient thermal resistance value under the condition that thermal pad is connected to the copper plane, please tell me the thermal resistance under the condition that it is not connected.
(If the characteristic value of thermal resistance at this condition is clarified)
The usage conditions of DAC8760 are shown below as reference.
- The DAC8760 will use only voltage output function.
(Does not use current output function of DAC8760)
- The bottom of thermal pad does not connect to AVSS copper plane.
(The AVSS pin (1pin of HTTSSOP package) is conncted to negative supply voltage)
- Volatge output pin of DAC8760 is connected to input pin of external opeamp circuit.
(Connects to high impeedance input)
Regards,
MESH