Other Parts Discussed in Thread: ADC12J4000, TRF3765
Hi, I am using an ADC12j4000 along with a tswj1456EVM to capture some RF measurements. I have a signal generator generating a 1GHz signal and when looking at the data I am seeing large amounts of ripple in the measurements (around 2.7dB). Is this a known issue or am I doing something incorrectly? Is 1GHz too high of a signal to put into the ADC12J4000 EVM? The measurements I have below are CW signals but I see the exact some behavior in pulsed measurements as well. One thing I found strange is 1GHz is very rippley, but 900MHz is not. In fact, multiples of 300MHz look ok. Is there anything that I can do to mitigate this ripple? I have done this with a narrow bandpass filter as well but still see the same results.
Thanks for your time,
Kyle
1GHz CW signal 900MHz CW signal