Part Number: ADC3221
Other Parts Discussed in Thread: THS4541
Hi team,
Can you have a look at the following customer question and suggest an opamp, please?
For a current project I am currently looking for a measurement technique with 12-ADC and >=25MHz for 2 channels (simultaneous).
A passive anti aliasing filter is planned (calculated with Ri = Ro = 50Ohm).
Draft of the block diagram

One possibility would be the ADC3221.
Analog input voltage range +/-0.5V - so the voltages from above are to be halved.
Or not?
Here is an extract from the datasheet:

Is the specification 2-Vpp correct? Does this specification refer to the input at the ADC?
Which amplifier(s) would you suggest for this application?
Thank you,
Franz