hi,
i want to use this ic,but i am getting to which controller pins i need to connect clock and data pins. i am using MKE16Z32VLF4 controller.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
i want to use this ic,but i am getting to which controller pins i need to connect clock and data pins. i am using MKE16Z32VLF4 controller.
Hi Uma,
I do not see a peripheral on your processor that is able to accept the bit-stream output of the AMC1204. The performance specified in the AMC1204 datasheet is based on using a Sinc3 filter with a decimation ratio of 256. If you controller has similar features, there should be documentation from the manufacture on how to set that up and which pins you should use.