Part Number: ADS1258
Hi,
I am working with an ADS1258 and had a question about the DRDY signal. I have four ADS1258 with the SPI interfaces all on the same bus, using the chip select to read each of them. I fan out the start signal to all four ADCs and then read them when I receive the DRDY. My question is, will the DRDY clear (go back high) on the falling edge of SCLK if the ADC chip select is not low? The reason I ask, is I need to know if I should wait for all the ADC DRDY signals before reading each of them.
Thanks,
HSG