Part Number: ADS4222
Other Parts Discussed in Thread: THS4521,
Please see below schematic.
1) Is Rload required for the design?
2) Is two Ro (49.9 ohm) required for the design?
3) How to decide the resistor value for Ro and Rload?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shen,
Determining the RLoad for this type of interface, can be found in the THS4521 datasheet. This amplifier was characterized under a 1kohm load differential. So it is best to use a combined resistor network that reflects an Rload of 1kohm in order to achieve the best performance out of the amplifier.
Regards,
Rob
What does 1K load means in my circuit?
The ads4222 differential input resistance is 0.75kohm.
So should set Ro = 0.25kohm and Rload= Not installed ?
Hi Shen,
I would put Rload, then put some additional series resistance near the analog inputs. ~5-15ohms, after Rload.
The equivalent resistance should be roughly1kohm differential for the amplifier. But its not an exact absolute requirement.
Also, I would look at Table 4 & 5 on page 24 of the THS4521 datasheet, this will also give some guidance on the resistor values based on the amplifier gain and input configuration that will be used in your application.
Regards,
Rob
Hi Rob,
I would put Rload --> what does it mean? installed or remove? if install, what resistance value should be installed?
I don't understand how do you achieve 1K ohm based on above comments, 49.9 ohm + 5~15 ohm + 0.75Kohm ?
Hi Shen,
I apologize for the confusion, 1Kohm was just an example.
The resistor value would be dependent on the gain and input configuration you plan to use for your application.
Once we know those, we can use the tables (4&5) in the THS4521 datasheet to determine the resistor values needed for the interface.
Regards,
Rob
Hi Rob,
The table 4&5 is for Rf and Rg. I think it's different from our topic about the output interface with ads4222.
What I want to know the resistor value Ro and Rload setting between THS4521 and ads4222?
by the way, my application is using single end and 1 Gain.
Hi Shen,
thank you for the information, this helps.
Last question before I can recommend a circuit for you.
Do you plan to DC couple between the output of the amplifier and inputs of the ADC?
Or AC couple, ie - use an AC blocking cap to break the VCM differences between the amp and ADC?
Regards,
Rob
Hi Rob,
Thanks for much detail explanation.
So the target is to set Rb//Radc = about 1K ohm, is this understanding right?
One more, what's the purpose of Ra and Rc?
Hi Shen,
yes, that is correct, set Rb//Radc = about 1K ohm.
Ra will help with any parasitic C on the output of the amp. This will help dampen the response and prevent any oscillations which can sometime occur.
Rc will help with any charge injection/kickback from the ADC's internal sampling cap.
Here is a good link that describes this in more detail, also look at reference 10 and 11.
www.electronicdesign.com/.../dissecting-the-highspeed-amplifieraafadc-interface
Regards,
Rob
Hi Rob,
Should I reserve capacitor like below? Make sense or not?
My application is 50M sample rate.


Hi Shen,
Either configuration is fine to filter out the wideband noise.
Regards,
Rob