Part Number: ADS124S08
Using the ADS124S08. I am able to write all registers and control the ADC via SPI. I am currently connected to AIN0 for positive and AIN1 for negative of a differential signal.
I am set to use REF0 for my reference that is 5V (AVDD)
I am able to read a -0.038V signal with PGA of 1 accurately. I am able to read the voltage with a PGA setting of 2 and it reports twice the ADC counts. Higher PGA settings cause the ADC to lock up for lack of better description. I can lower the voltage closer to zero and get it to work. What am I missing on how the PGA works, I thought a setting of say 4 would simply take the ADC reading and return 4X the counts thus stating the voltage as 4X the input value and that would be -0.038V X 4 = -0.152V. Perhaps I am missing how the PGA actually works or am I up against a voltage to reference limitation?