Other Parts Discussed in Thread: ADS1298
Hi,
What is the expected DVDD current on the ADS1298ECGFE evaluation board when configured for 3.3V operation using JP24?
- When the PWDN jumper (JP5) is attached, I measure DVDD = 20.6 mA & AVDD = 4.98 mA
- When the PWDN jumper is removed, I measure DVDD = 20.5 mA & AVDD = 1.26 mA
The DVDD current is well outside the value listed in the ADS1298 electrical characteristics. It is always measures high regardless of the operational state of the device.
Other than this the device appears to be fully functional.
What would be the cause of the high current?
Thanks
-Chris